3/2/2009 8:34 AM | |
Joined: 5/12/2006 Last visit: 10/19/2024 Posts: 22422 Rating: (3023)
|
Hello, 3.) Upload of the project is available with SIMOTION V4.1.2.0 refer this thread: /tf/WW/en/Posts/23729 2.) no "extra" procedure is need. compile all programs, check consistency and download the project. 1.) HWChanges can be download via HW Config or NetPro. But the better way is to download any changes via Scout, because there any other data which can be modified (adresses of TO's) when you make chances in hwconfig. Regards Christoph |
3/2/2009 2:13 PM | |
Posts: 8 Rating: (0) |
Wow..fast reply.. i Really appreciates with the answer. Thank you very much |
Follow us on