11/10/2020 11:54 AM | |
Joined: 10/10/2014 Last visit: 8/28/2024 Posts: 1725 Rating: (210) |
Hi leem2209,
Best regards |
This contribution was helpful to1 thankful Users |
11/10/2020 4:16 PM | |
Joined: 4/18/2017 Last visit: 3/24/2024 Posts: 29 Rating: (0) |
One thing I couldn't figure out from this manual was how to call one function from another. Unless I missed it somewhere, it didn't actually give any examples of how to call another function or sub from an action. But this put me on the right path of where to store the VBS scripts and some googling later got me understanding calls and passing over variables. |
11/11/2020 8:14 AM | |
Joined: 1/15/2018 Last visit: 8/27/2024 Posts: 145 Rating: (5) |
Hi leem2209, You just need to write the name of the function or call "name_function" where you want to call it. Note that you can use input tags on the function and return values on the case. For it, you need to define you function as function and not sub... For example: Normal function:
Function with input tags:
Function with output tags. You need to define it as fuction. Name of the function is the tag return:
How to call a functions from other function or action:
Best regards, Gonzalo |
Last edited by: gjimenez at: 11/11/2020 08:15:45Last edited by: gjimenez at: 11/11/2020 08:16:49 |
|
This contribution was helpful to1 thankful Users |
Follow us on