2/2/2022 8:03 AM | |
Joined: 10/30/2018 Last visit: 9/13/2024 Posts: 11 Rating: (0) |
Hello to all. I want to make changes to an uploaded application, but I get the following errors. 1- I want to add FB39 to the program and call it in FB20, FB39 is created without any problem but I can not define it as a STAT in FB20 and the diclaration table turns red and the Update declaration option does not work (photo No. 1) 2- In order not to face this problem, I skipped adding FB39 and logically added it at the end of FB38, which is actually a copy of each other, and after SAVE it, I realized that in FB20 again for STAT0 (defined for FB38) The diclaration table error has occurred, if it did not already have an error. (Photo No. 2) Please guide me so that I can solve this problem. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/02/2022 09:52:15New subject after splitting |
|
2/2/2022 8:28 AM | |
Joined: 10/30/2018 Last visit: 9/13/2024 Posts: 11 Rating: (0) |
here is Foto No.2 |
2/2/2022 3:46 PM | |
Joined: 10/30/2018 Last visit: 9/13/2024 Posts: 11 Rating: (0) |
Hi Jacked, yes it does. |
Follow us on