2/21/2024 11:17 AM | |
Joined: 12/4/2023 Last visit: 4/11/2024 Posts: 4 Rating: (0) |
Dear All, I am having a issue where my web server displays and functions correctly without issue on the pc. Analog Values & Scale Times are updated and submitted for the relevant fields using "Enter" and then gets the good old "submitted" in red display. I have however come across an issue when accessing the same from mobile phone. Everything displays correctly but I am unable to update all the writable fields. I am only able to update the very last input box on my page and whenever trying any of the other input boxes, the enter button just makes the cursor jump to another input box with no information being updates on the box that was edited. I have tried editing the render.js with updated to the relevant renderJs.initialAnalogInputComp function where keydown, focus etc. is specified. I went as far as to verify a mobile device and to do a prevent default event to see if it helps to no avail. Has anybody come across the same issue, am I missing something or doing it incorrectly? I have attached my files for any feedback AttachmentWaterscheme LWE + LSC.zip (152 Downloads) |
2/21/2024 1:05 PM | |
Joined: 12/18/2014 Last visit: 5/17/2024 Posts: 33050 Rating: (4082) |
I can only say that Android OS is the problem. You can start a Support Request and ask Siemens directly for help. |
This contribution was helpful to1 thankful Users |
2/21/2024 1:09 PM | |
Joined: 12/4/2023 Last visit: 4/11/2024 Posts: 4 Rating: (0) |
thank you. I do appreciate your input |
Follow us on