5/21/2020 10:24 AM | |
Posts: 5 Rating: (0) |
Hello, how can I change the X30 COM to Modbus RS485 ? The first question is of course which ttySx is used ? Is "switchserialmode /dev/ttySx rs485" command right ? I have compiled the image from the github: https://github.com/siemens/meta-iot2050 and "iot2000setup" is not included, will this come later? This is my first post here, I hope that in the future I can contribute more than asking questions :) |
Last edited by: oxinon at: 05/21/2020 10:25:28 |
|
5/21/2020 5:38 PM | |
Joined: 3/17/2014 Last visit: 10/7/2024 Posts: 53 Rating: (12) |
Hello oxinon, iot2000setup now is become iot2050setup. Type it and then you have almost the same menus from iot2000setup. For Serial Port go in Peripherals --> Configure external COM port Hope can it help BR |
Last edited by: davide_maffei at: 05/21/2020 17:38:45 |
|
5/22/2020 1:48 PM | |
Posts: 5 Rating: (0) |
Yes helped me switch to RS485, but which ttySx is used for X30 COM? question is solved to 50% Thanks! |
Follow us on