12/20/2020 7:51 PM | |
Joined: 3/15/2018 Last visit: 1/9/2024 Posts: 25 Rating: (0) |
Hello Guys, I have a problem with Simotion D445-2DP/PN. It keeps stopping with all LED lights flashing red, after restarting the module it works normally for less than 30 minutes and the same problem continue. I uploaded the station and the following errors occurs each time the problem happens: Event details: 1 of 202 : 12:33:30:975 am 07/07/92 Event ID: 16# F360:2425 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 11: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 2 of 202 : 12:33:30:975 am 07/07/92 Event ID: 16# F360:2424 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 10: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 3 of 202 : 12:33:30:967 am 07/07/92 Event ID: 16# F360:2423 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 9: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 4 of 202 : 12:33:30:967 am 07/07/92 Event ID: 16# F360:2422 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 8: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 5 of 202 : 12:33:30:959 am 07/07/92 Event ID: 16# F360:2421 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 7: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 6 of 202 : 12:33:30:951 am 07/07/92 Event ID: 16# F360:2420 Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 6: Fault number 35220, fault value 0x4000 Incoming event ................................................................................ Event details: 7 of 202 : 12:33:30:943 am 07/07/92 Event ID: 16# F360:241F Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 5: Fault number 35220, fault value 0x4000 ................................................................................ Event details: 8 of 202 : 12:33:30:935 am 07/07/92 Event ID: 16# F360:241E Additional information 4 / 5: 16# 00 00 Additional information 1 / 2 / 3: 16# 8994 0000 4000 Fault DO 4: Fault number 35220, fault value 0x4000 Incoming event ...................................................... I attached the diagnostic buffer log below Please help and advise Thanks and regards Attachmentdevicediagnostics.pdf (654 Downloads) |
12/21/2020 3:09 PM | |
Joined: 3/15/2018 Last visit: 1/9/2024 Posts: 25 Rating: (0) |
Hello Christoph, the disply in the D445 shows F when the error occurs. i take the attached diagnostic buffer directly from the accessable nodes. note that each time the problem occur the D445 all LEDs flashing red and the module kicks all the communications eith profibus or profinet and feels just like it went power off. i hope all this can be helpful to diagnos the problem Attachmentdevicediagnostics.pdf (685 Downloads) |
12/21/2020 3:11 PM | |
Joined: 3/15/2018 Last visit: 1/9/2024 Posts: 25 Rating: (0) |
attached, Screenshot of TM41 alarms which same in 8 axises |
12/21/2020 3:12 PM | |
Joined: 3/15/2018 Last visit: 1/9/2024 Posts: 25 Rating: (0) |
attached, TM41_Axis_0 online values from expirts list AttachmentTM41_Axis_00_Online Vaues.pdf (571 Downloads) |
12/21/2020 3:13 PM | |
Joined: 3/15/2018 Last visit: 1/9/2024 Posts: 25 Rating: (0) |
attached, Dp6 drive axis 7 online values from expirts list AttachmentDP6_Axis7_experts_List.pdf (550 Downloads) |
12/22/2020 5:52 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
hi, hello first you should use the latest V4.4 (HF18) . simple copy /paste the FW on the CF Card (Remove the old FW before, delete all expect the keys aqnd user folder) Download FW: |
Follow us on