3/22/2022 3:11 PM | |
Posts: 17 Rating:
|
Good afternoon. How do I convert txt file to dnl? ------------------------------------------------------------------------------------------ |
Last edited by: pirulas at: 03/22/2022 15:11:44Last edited by: Jen_Moderator at: 03/23/2022 09:47:51New subject after splitting |
|
3/23/2022 4:00 PM | |
Joined: 6/4/2008 Last visit: 8/5/2025 Posts: 1518 Rating:
|
Hi, easy and free using windows file explorer, copy or move the file to an easy to find location like the root of your C drive (C:\) rename the file to something easier like compressor.txt Then as per the attached screengrabs, type in CMD into the run entry field and click on Command Prompt. change the directory to where you have moved the file (i.e. root) by typing in CD \ rename the file extension by typing in the command as seen (ren means rename) OBVIOUSLY, replace filename with the name of your file. Hope this works OK Regards, Graeme Attachmentrename.zip (824 Downloads) |
Last edited by: Graeme at: 03/23/2022 16:37:47 |
|
3/28/2022 8:15 AM | |
Joined: 3/25/2008 Last visit: 9/15/2025 Posts: 224 Rating:
|
hi, nothing is converted, just rewrite the .txt extension to .dnl |
Follow us on