Industry Online Support
Technical Forum
12/27/2006 10:36 AM | |
Posts: 8 Rating: (0) |
Hi, I'm a student of University of Brescia, we have bought from Siemensthe "SIMATIC NET: DK-ERTEC 400 PNIO", that it comprises: - "DK-ERTEC 400 PNIO V2.0" 6 "Tornado 2.2.1/VxWorks 5.5.1" sw - "SIMATIC NET: DK-16xx PN IO V 1.0" & V 2.0 sw - "Development kit for PROFINet IO V 2.0" sw - "SIMATIC NET: CP 1616 V1.0" & V 2.0 sw - Evaluation Board ERTEC 400 PNIO (as device IO) - CP 1616 (as controller IO) I'm following the instruction of manual, and soI'm tryingto install Linux Suse9.3, but I have a problem: I download from internet (Suseorg.com) the ISO cd of Linux, and we have so a version 2.6.11.4 of Kernel (Instead 2.6.10); so we have used this file for configuration: - "linux-2.6.11.4.tar.bz2" instead of "linux-2.6.10.tar.bz2" - "adeos-linux-2.6.10-i386-r12.patch", whichI find at http://download.gna.org/adeos/patches/attic/v2.6/i386/instead - "rtai-3.2.tar.bz2", that my pc save as "rtai-3.2.tar.tar" It's right? I have some problem:they are successful to install the kernel, but in the moment in which I install the RTAI appear of the errors erorr display: "structure has no member named 'used_math' " and after "install-recursive Error 1'"... |
12/29/2006 8:31 PM | |
Joined: 9/1/2005 Last visit: 10/14/2024 Posts: 4109 Rating: (195) |
Closed: cause thread was posted twice. The other thread you can find here: SUSE 9.3 and RTAI INSTALLATION. |
My Forum is the place to personalize your profile, |
|
Follow us on