6/29/2009 8:26 PM | |
Posts: 1 Rating: (0) |
Dear all
We are AL SHAHEED GENERAL COMPANY, one of the companies affiliated to the Ministry of Industry and Minerals in Iraq. Our company is located in the province of Anbar – Iraq.
within the plant to produce copper In fact, we suffer from a rise in vibration motor manufacturing SIEMENS the date information on name plate as following: Serial Number: 1-5113-65103-1-1 Type: RAZ Frame: 509 US Model: 149 RPM: 2970 H.P.: 400 Operation instruction: M3115
But the bearing is not understand or unknown
Shaft End Bearing: 75 BCO 3x3 Shaft Opp Bearing: 75 BCO 2x3
So we need for assistance for select of size and type bearing
At End, we wait your replay
Best regards
Photo PDF attached shows the work of motor
AttachmentMotor.pdf (219 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on