7/3/2007 2:31 PM | |
Posts: 6 Rating: (0) |
Hi all, after a problem during configuration transfert from Step 7 (5.4 sp2), my CP1616 is OFF. More details: -CP1616 is configured as controller with 2 devices (ET200S). - SF led is lit (ON) - BF led is blinking - I can't ping the CP1616 when I start any software under my Linux RTAI I have the status 0x30D (PNIO_ERR_CONFIG_IN_UPDATE) If I try to change the firmware with SIMATIC NET firmware - Loader through ISO protocol, an error occur : action is Deleting old firmware. I use the Mac addressprinted on the CP1616. I don't use MAc address +1 because I have no answer on the cable (see with Wireshark) Who can help me? |
Follow us on