Industry Online Support
Technical Forum
10/10/2011 12:45 PM | |
Posts: 10 Rating: (0) |
Hello, Thank you for your reply, I know that you say mark the objects and create faceplate by the right click I want to learn how can I connect the tags. In WinCC 7.0 I do like that: First of all, I write a FB for example a valve. then I call this FB e.g. in OB1 so the instance DB is created. (you can see it "db.jpg" in fp.zip in attachments) Then I create the structure data in winCC according to this DB (you can see it "structure.jpg" in fp.zip in attachments) After thatI call the structure type ine.g TCP/IP->New Connection->Tags So the tags are created. (you can see it "tags.jpg" in fp.zip in attachments) Lastly Ido faceplate. For a faceplate I insert a new PDL from graphics designer so I design the picture. After the design I connect the tags properly. Thus I write the part of the tag for example ".Limit_open" (you can see it "fp.jpg" in fp.zip in attachments) So when I click the symbol of valve, the other part of the tag is loaded. Example we have 3 valve. And their names are valve1, valve2 and valve3 if I click the first valve the tag is "valve1.Limit_open" if I click the second one the tag is "valve2.Limit_open" And So WinCC 11.0 I write a FB for example a valve. then I call this FB e.g. in OB1 so the instance DB is created. (I DID IT) Then I create the structure data in winCC according to this DB (I create new data type from the libraries menu) (you can see "datatype.jpg" and"datatype2"in fp.zip in attachments) (I DID IT) After that I call the structure type in e.g TCP/IP->New Connection->Tags So the tags are created. (I create the tags to the tags menu) (you can see "datatype5.jpg"in fp.zip in attachments) (I DID IT) Lastly I do faceplate. For a faceplate I insert a new PDL from graphics designer so I design the picture. After the design I connect the tags properly. Thus I write the part of the tag for example ".Limit_open" (ı design the faceplate and mark the objects then create faceplate by right click. My problem is here.How can I connect tags? If you look over the "datatype31.jpg" in fp.zip in attachment you may see my problem. I can not choose the wincc datatype. I only choose flexible data type. So it is not work. Thank you for your help Attachmentfp.zip (1012 Downloads) |
Follow us on