Industry Online Support
Technical Forum
5/15/2010 1:24 AM | |
Joined: 9/27/2006 Last visit: 11/13/2024 Posts: 12293 Rating: (2691) |
Hello jaykarnik; Quick answer: yes, it is possible to control multiple motors with one drive. The devil, as usual, is in the details, Output current, total power, motor cable length,line chokes and individual motor protection are all things that you will have to look into for this application to work. Have a look at the following discussion, especially the Siemens FAQ that is quoted towards the end. Things should be a little bit clearer: /tf/WW/en/Posts/18410 Hope this helps, Daniel Chartier |
5/15/2010 3:05 PM | |
Joined: 9/27/2006 Last visit: 11/13/2024 Posts: 12293 Rating: (2691) |
Hello Jay; Here is a link to Leeson's drive FAQs: http://www.leeson.com/TechnicalInformation/faqdrives.html Hope this helps, Daniel Chartier |
Follow us on