10/12/2015 12:44 PM | |
Posts: 1 Rating: (0) |
Hi! Recently we've mounted Mag 3100 Sensor and MAG 6000 transmiter. After I enter parameter value on transmiter, I checked flow rate. The method of mesuring is as bleow. 1. pump start. 2. After 10 min, I stored the liquid for 1 min. 3. After that, I compared mesuring value on display of transmiter with real volume of Iiquid (alum) I stored. But the value is difference. -. Mesuring value on display : 9.4L per min -. real volume of Iiquid I stored : 4.4L per min I don't understand why the value is difference. The transmiter doesn't display alarm information. I attached file about regarding flow sensor installation on site. Could you tell me what I'm should do first? Thanks in advance for support.
AttachmentFlow_Sensor_Installation.pdf (152 Downloads) |
Follow us on