6/4/2020 1:25 PM | |
Joined: 8/3/2009 Last visit: 10/8/2024 Posts: 13877 Rating: (1751)
|
Hello It depends on which Logging format you want to use. If you can work with the logging in WinCC Advanced then I would use this (but then the csv file format is fixed). Here you can use the On Demand Trigger and the Systemfunction LogTag. Of course you can also use a userdefined Script. then you can program how your csv File should look like: https://support.industry.siemens.com/cs/ww/en/view/106501825 There is also a poosibility on PC Systems with installed MS Office to use the MS automation Interface in Script to write directly into xls File. Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/27/2024 3:49 AM |
|
Joined: 9/5/2022 Last visit: 10/2/2024 Posts: 1 Rating: (0) |
Run that script in event |
Follow us on