5/25/2022 8:44 AM | |
Joined: 7/20/2006 Last visit: 5/23/2024 Posts: 128 Rating: (8) |
Hi, I didn't want to open new topic, so I will ask here, because question is around this topic. I am preparing upgrade system from V7.1SP3 to V9.1SP1. My question is which steps do I need to follow. According: to Process control system SIMATIC PCS 7 Software update with utilization of new functions V9.1 SP1 https://support.industry.siemens.com/cs/document/109809169/simatic-process-control-system-simatic-pcs-7-software-update-with-utilization-of-new-functions-v9-1-sp1?dti=0&lc=en-WW I need to start from version V7.1Sp4 and that I have already done - conversion from SP3 to SP4. My question is if I can go direct to V9.1SP1 or I need to make some between steps, like conversion to v8.2. Manual is not so clear about that. regards Edek ------------------------------------------------------------------------------------------ |
Last edited by: edek at: 05/25/2022 08:44:42Last edited by: edek at: 05/25/2022 08:45:21Last edited by: Jen_Moderator at: 05/25/2022 10:13:44New subject after splitting Last edited by: edek at: 05/25/2022 10:45:11 |
|
5/30/2022 12:02 PM | |
Joined: 1/11/2019 Last visit: 5/31/2024 Posts: 715 Rating: (140)
|
Hello edek, This section informs you about the service for upgrading various previous versions of SIMATIC PCS 7 as well as the version-specific use of software and licenses for system communication via Industrial Ethernet: The range of upgrades is divided into:
You must Upgrades from SIMATIC PCS 7 Version V7.1 to Version V8.2 In your case before getting into PCS7 V9.1 Manual for Migration to PCS7 V9.0- In this forum query, users have given their inputs to upgrade the PCS7 version from V7.0 to V9.0. And, Follow the "Process control system PCS 7 Software update with utilization of new functions V9.1" Manual to upgrade it to V9.1 Hope it helps you! |
5/31/2022 12:18 PM | |
Joined: 1/11/2019 Last visit: 5/31/2024 Posts: 715 Rating: (140)
|
Hello edek, Usually in the upgradation perspective, there are two options: with or without the utilization of the functionality of the newer version (9.1 in this case). It is recommended to go through this manual perform the upgradation based on your requirement. SIMATIC Process control system PCS 7 Software update with utilization of new functions V9.1 Below points are for PCS7 V9.1 SP1 upgradation Manual software with utilization of new function can only works with PCS7 V7.1 SP4 or higher projects If you don not want to utilize the new function. i.e., Manual software without utilization of new function then you must have PCS7 V8.2 SP1 Project with you. But, in your case. You have Project with PCS7 V7.1 SP3. Hence, Please upgrade it to PCS7 V8.2 SP1 in order to upgrade it to 9.1 or to 9.1 SP1 |
This contribution was helpful to2 thankful Users |
Follow us on