5/8/2024 1:07 PM | |
Joined: 8/3/2009 Last visit: 10/8/2024 Posts: 13876 Rating: (1751)
|
Hello xsmart If there is/was no Image Folder on the 2nd PC then I suppose there has to be something wrong with the installation... I think since TIA V16 there is the need to install the Images seperate from the FAQ download (LINK) In V15/V15.1 the Images should be installed at installation and then if you install an Update for TIA Portal. I checked installation and here you can activate the Panel image: Perhaps this was missed in the installation on PC2 Then there are also more files for the transfer than only the image file. I would try to modify the installation, activate the current Panel images and then install the Upd6 for V15.1 again I´m not sure if this is the issue in your situation but it would make sence Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on