5/7/2024 10:49 AM | |
Joined: 5/30/2022 Last visit: 7/5/2024 Posts: 548 Rating:
|
Hi Tejus, You would have to check that it pings between the PC and the PLC and verify the PG/PC interface setting: Setting the PG/PC interface for WinCC communication with the controller And that the application access point configured on the link in TIA Portal, matches what is configured in Interface PG/PC. |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to
1 thankful Users |
Follow us on