11/15/2019 11:45 AM | |
Joined: 11/29/2017 Last visit: 9/4/2024 Posts: 19 Rating: (0) |
Hi, I loses the connection between the PLC en WinCC sometimes. In the attachement you find the hardware setup and how i set my connection in WinCC. I already did the following:
Now point 4 was only when i called a global script (vbs and i called a script with nothing in it to be sure it was not the script) through a tag from the list of the problematic PLC. Also when i called a global script through a Cyclic Timer and know i read or write a tag from the problematic PLC the connection also got disconnected. So i don't know what else i can look for. Anybody an idea? Also the connection to the PLC go through a CP 343-1 Lean card. Can this be the problem maybe. Thans in advance.Kind regards, Ward AttachmentSetup PLC.zip (585 Downloads) |
1/14/2022 1:37 PM | |
Joined: 10/4/2021 Last visit: 3/27/2023 Posts: 24 Rating: (0) |
Hello I again got the disconnection in different WinCC in kog files the error code is 8104. |
Kamil Ibadov |
|
Follow us on