3/16/2017 2:46 PM | |
Joined: 10/18/2006 Last visit: 7/31/2025 Posts: 120 Rating:
|
Hi chikhim, you are using the connection mode "TCP S7-1x00". The performance is less compared to "TCP/IP". But in fact I would expect a better update time with so few signals. What is your configured update time in S7-Xplorer? And please check the "communication load" setting in the Device configuration of your CPU1516. The default is 50%. Are you using HMI devices? Is the ibaPDA performance getting better if you disconnect them? |
iba AG - Data Acquisition and Analysis the way it should be |
|
This contribution was helpful to
1 thankful Users |
Follow us on