3/28/2023 3:37 PM | |
Joined: 10/28/2019 Last visit: 12/15/2023 Posts: 27 Rating: (0) |
Good afternoon, I used a 250 GB card in standard format. Since then the logo fails me, I can't communicate via ethernet, I've started to put the factory settings on it and I couldn't, the factory settings don't appear, I've tried admin and operator and I can't find the factory settings. Thanks and best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/29/2023 04:11:09Text formatting optimized. Last edited by: Jen_Moderator at: 03/29/2023 04:13:35New subject after splitting |
|
3/28/2023 4:05 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191)
|
In attachment the menu structure of the LOGO!. The menu point "Factory Reset" find you in the setup menu. But this menu point can you only see in Admin mode. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0.pdf (364 Downloads) |
4/1/2023 11:28 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191)
|
The LOGO! with the firmware V1.08.02 is a LOGO! of the first generation, a LOGO! 8.0. And the LOGO! "Reset Tool" is only for the current LOGO! 8.3. AttachmentVersions of 0BA8.txt (388 Downloads) |
Follow us on