6/25/2010 2:59 AM | |
Joined: 10/7/2005 Last visit: 7/14/2024 Posts: 3009 Rating:
|
Hello FrozenWaves not too sure if a codeexample exist for rotational speed measurement mode of the ET200S 1 Count, but the various modes that this card can operate in arequite well explained in the following manual (just in case you do not have it yet): ET200S Technological Functions Note that you'll find the same 1 Count module part number generally TWICEin the HWconfig catalogue. One has a"C" at the end of the part number (to be used if counting mode is to be configured) and the other has an "M" at the end of the part number. You'll need to select and drag the"M" suffixed part number of your 1 Count card into your ET200S station to configure it for measurement mode. And to make things even more "challenging" concerning the correct selection in HWconfig: Certain 1 count cards also support "position feedback mode" which makes them also appear with a "W" suffix and the latest 1 Count cards withFirmware version 2 now also supportso called "Fast mode", so thisone appearsa total of 4 times in theFunction module sectionof the ET200S (see THIS link for more on fast mode). I hope this helps |
Cheers |
|
Follow us on