7/27/2010 10:24 PM | |
Posts: 28 Rating:
|
Dear friend jklm I dont understand way you said once WinAC and lather Win LC Beacause you have said also "same configuration" - is correct or is a typing mistake ? I try to create a software PLC with WinLC and CP 5611 connected by Profibus to ET 200U module. It seems that I have no communication on profibus network. I had called the OB81, OB82, OB83, OB85, OB87, OB122, FC1, FC2. The CPU is on running mode, but, I am stuck with SF ON and BUSF1 LED blinking. I had try with another computer to connect to this Profibus network, but it seems to not be active. I try to monitor the FC1 but the status code seems to not access address 3 that I set to ET200U. Can you suggest what speed is ok for ET200U. I do not found documentation for this old module. Please share your experience. Any suggestion would be appreciated. Also a small PLC program as example will be a good reference. Best regards, dekor. Splitted from can we replace win AC slot PLC, into win LC+CP ?. |
Last edited by: O_Moderator at: 7/29/2010 7:58 AMnew subject after splitting |
|
7/29/2010 8:00 AM | |
Posts: 378 Rating:
|
Hello, i don´t know much about this topic, but maybe thia manual could help you. http://support.automation.siemens.com/WW/view/en/1142468 Good luck Bilao |
7/29/2010 4:14 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello dekor; We recently had a discussion here on the same subject: /tf/WW/en/Posts/46450 The conclusion was that only an interface module -8MB13 would connect properly to a Profibus-DP network. What are the part numbers for your IM 318C modules? Hope this helps, Daniel Chartier |
8/4/2010 4:48 PM | |
Posts: 28 Rating:
|
Dear friends, thanks for links and suggestions. I will change the module also. Maybe is defective.... dekor |
Follow us on