10/2/2008 2:02 PM | |
Posts: 13 Rating:
|
Hi Can anyone tell me where I can find GSD files voor VS723A and VSLink for Profinet. greetings Anjenny |
10/2/2008 3:59 PM | |
Posts: 103 Rating:
|
The VS723A is Profinet ready and the file is a GSDML in .xml format. I believe it comes with the Spectation software. The VSLinkwas (now obsolete) designed to display a VGA image extracted from the Ethernet communication of the VS72x. It was also available with a Profibus option to pass values to a DP network. There is now an option for WinCC Flex to embed control and images directly from a camera into the HMI. --> 6GF8007-4AA20-0AB0 I got around this using a different brand of camera (Sorry Siemens,I already owned it)that was based on the same technology by serving a webpage from the camera and viewing it in a html window on WinCC Flex. I have attached the xml file for the VS72x and the gsd file for the VSLink (I believe they are the correct versions but you will have to check) AttachmentFilesZipped.zip (238 Downloads) |
Follow us on