8/22/2009 1:46 PM | |
Joined: 10/7/2005 Last visit: 8/9/2024 Posts: 3016 Rating: (1054) |
Hello Genious Brain which which type of Profibus comms have you set up between the DCS and the S7? Most likely candidates are DP-DP Master comms via DP coupler OR DP Master - DP Slave comms (there are other possible Profibus comms available butgut feeling tells me it is one of the two above and I'd be interested to know anyhow which way you went concerning THIS thread). Anyway,either way it is really just a matterof checking/determining the data mapping (i.e. which I/O's on one side correlate to which I/O's on the other side. Onceyou did this you'll know where the bits come from. Should you have problems finding out what writes to theOutput addresses in the S7, I suggest you post the S7 program here together with info theoutpput addresses. I hope this helps |
Cheers |
|
Follow us on