6/4/2024 12:02 PM | |
Joined: 6/4/2024 Last visit: 6/5/2024 Posts: 1 Rating:
|
Can you guide me how to use Profinet and Modbus TCP in 1200?? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/05/2024 06:57:16New subject after splitting |
|
6/6/2024 5:05 AM | |
Joined: 3/11/2019 Last visit: 7/9/2024 Posts: 1511 Rating:
|
Hi, any "specific" question or error? In general, both can be used in parallel. Configure your profinet io devices like you would without Modbus TCP. Configure your Modbus TCP instructions like you would without profinet. There are also some application examples for Modbus TCP in SIOS/SiePortal available. You can also use the examples for S7-1500, the instructions are the same. For everything else, please be more specific. Better questions led to better answers. How do you program and parameterize Modbus/TCP communication between S7-1500 CPUs and S7-1200 CPUs?How do you program and parameterize Modbus/TCP communication between two S7-1200 CPUs?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
Follow us on