6/16/2010 2:48 PM | |||||||||||||||
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating:
|
Hello Solution Riders: Here is information gathered from different sources: 1) From the ET 200S IM151-1 Standard interface module manual, Chapter 1, Properties of the module: http://support.automation.siemens.com/WW/view/en/25548014 Insulation test voltage 500 VDC Current consumption from rated supply voltage (1L+)Approx. 200 mA Power dissipation of the moduleTypically 3.3 W 2) MLFB 6EP0133-3AA00-0AA1 is notcurrentin the Siemens A&D Mall
Hope this helps, Daniel Chartier |
||||||||||||||
This contribution was helpful to
1 thankful Users |
Follow us on