7/27/2006 4:58 PM | |
Joined: 5/24/2006 Last visit: 11/14/2007 Posts: 93 Rating: (4) |
Hi J_Bell, so, do you even use OSM to perform direct link with DIGSI via Fibre Optic in switch operating mode? My main concern is by using OSM, whether it's possible to get the communication between DIGSI program in PC and SIPROTEC device in another end. Attached a ring sturcture that i've plan to work on. kee AttachmentCan DIGSI runs on the Notebook via the above connection with.pdf (887 Downloads) |
Follow us on