9/13/2015 3:38 AM | |
Joined: 10/12/2014 Last visit: 2/27/2024 Posts: 66 Rating: (0) |
sir ; i m from sri lanka .I m working as a engineer in our company . Here i attached the error code image which is appeared in the Simatic panel .In simatic panel stop button also blinking . In this situation when I try to download the backup program , I cant proceed ,because when downloading the program using simatic manager it gives another error.Here i also attached the simatic manager error code image which appeared in the program. sir please help me to overcome with this fault. ------------------------------------------------------------------------------------------ Attachmenterror.zip (295 Downloads) |
Last edited by: Min_Moderator at: 9/13/2015 11:51:54 AMNew subject after splitting |
|
9/13/2015 11:55 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
The second thread with the subject simatic panel-c7 633 p error code($551 as address 2 not possible ) is published within the conference SIMATIC ProTool / ProTool/Pro. Best regards |
Follow us on