11/3/2023 5:27 AM | |
Joined: 3/7/2023 Last visit: 2/26/2024 Posts: 17 Rating:
|
Dear all I convert the project from S5 to S71200 . I already converted but some blocks are in STL Language that program i converted to Ladder but when i am trying to download and run the machine but the operation can't work . i miss some calculation from the Existing S5 program because i changed to ladder can you please help me to Convert this into Ladder. The existing they are using 2 High speed counter (IW106 and IW98) you can see it in FB53 and FB54.instead of that we are using the Inbuilt high speed counter . the problem is in the conversion of STL block and the Scaling for the new PLC.I have the problem with FB52,53,54,55,56 and FB197.Can anyone please convert this FB's to Ladder. Here i Attached the PDF of the Blocks. ------------------------------------------------------------------------------------------ AttachmentOB2.pdf (241 Downloads) |
Last edited by: Jen_Moderator at: 11/03/2023 10:41:14New subject after splitting |
|
11/3/2023 5:55 AM | |
Joined: 12/18/2014 Last visit: 6/17/2024 Posts: 33203 Rating:
|
Please don't post twice for the same problem. You also pst your problem in this topic: Convert S5 program into S7 Using S5 Converting tool
|
11/3/2023 10:47 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating:
|
Closed cause question posted twice. The second thread with the subject Need help to convert STL to Ladder is published within the conference STEP 7 (TIA Portal). Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on