11/25/2013 9:24 PM | |
Posts: 49 Rating:
|
hello I have a question, I am in the preparation of migration from S5 to S7 I exchange IP246 and IP247 modules. The IP247 modules (stepper motors) is for 24VDC control module (clock pulse, direction, etc. Connecting to power units with 24V optocoupler inputs). Is it possible to use the FM453 for such a stepper motor control module or only for 5VDC modules? ps. power unit is old BARGER LAHR D450.00 Attachmentstepper-motor_D450 -03_00002.pdf (490 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on