9/27/2021 9:50 AM | |
Joined: 12/1/2020 Last visit: 5/5/2025 Posts: 11 Rating:
|
Hi all I am converting S5 to S7, all program (attached) I have successfully migrated, not able to migrate FB210 of this program It is using indirect addressing. Can anyone help me? S5 program is attached. NAME: HANT.PCS DECL: UBDB B DECL: SEDB B DECL: RSET IBI DECL: EROR QBI DECL: RFLM QBI DECL: TIMT T DECL: TIMZ DKT DECL: INIT B DECL: COFF B DO =SEDB LW =SEDB SLW 8 SRW 7 L DW 72 +F LIR 0 T DW 70 LW =UBDB SLW 8 SRW 7 L DW 72 +F LIR 0 T DW 69 A =TIMT JC =M001 A =RFLM JC =M002 L KH 0000 OW JZ =M003 L KF -2 +F LIR 0 L KF +261 <F JC =M003 LW =TIMZ SD =TIMT L DW 69 L KF +6 +F T DW 68 DO =UBDB DO =INIT DO =SEDB L KH 0000 L DW 68 TIR 2 L KH 0400 L DW 66 AW ><F BEC S =RFLM JU =M004 M003: STS M001: S =EROR DO =UBDB DO =COFF DO =SEDB L KH 2000 L DW 68 TIR 2 AN =RSET BEC RB =RSET RB =RFLM A =RFLM LW =TIMZ SD =TIMT BEU M004: RB =RSET L KF +1 T DL 33 L KF +0 T DL 34 JU =M005 M002: L KH 8000 L DW 66 AW !=F BEC L KH 8000 L DW 67 AW !=F BEC AN =RFLM LW =TIMZ SD =TIMT A =RFLM LW =TIMZ SD =TIMT A =RSET AN =EROR JC =M004 RB =EROR L DL 0 T FY 253 L FY 253 L KF +1 !=F JC =M006 L KY 68,2 T FW 254 L KF +0 T FY 252 M013: L FY 255 L DW 70 +F LIR 0 T FW 250 L FY 255 L KF +2 +F T FY 255 L FY 253 L KF -2 +F T FY 253 L FY 250 SLW 1 L DW 69 +F T FW 248 M012: AN F 251.4 JC =M007 L FY 254 L DW 70 +F T FW 246 L FW 248 LIR 0 L FW 246 TIR 2 L FY 252 L KF +2 +F T FY 252 L FY 254 L KF +2 +F T FY 254 JU =M008 M005: JU =M006 M007: L FY 255 L DW 70 +F LIR 0 L FW 248 A F 251.5 JC =M009 LIR 0 AN F 251.6 JC =M010 AW JU =M011 M010: OW M011: L FW 248 M009: TIR 2 L FY 255 L KF +2 +F T FY 255 L FY 253 L KF -2 +F T FY 253 M008: L FW 248 L KF +2 +F T FW 248 L FY 251 L KF -1 +F T FY 251 L KH 000F AW JN =M012 L FY 253 OW JN =M013 L FY 252 OW JN =M014 L KF +2 T DL 34 L KF +1 M014: T DL 33 M006: L KH 8000 L DW 66 OW T DW 66 L KH 8000 L DW 67 OW T DW 67 BE
AttachmentCHIPPEST.zip (799 Downloads) |
9/27/2021 9:56 AM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
Please don't post twice for the same problem. You post also in this topic: conversion S5 to S7 (LIR and TIR)The moderator will close double postings. With double posting you make only more work for the moderator. |
This contribution was helpful to
1 thankful Users |
9/27/2021 10:44 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject How to convert LIR 0 and TIR 2 instructions? is published within the conference SIMATIC S5 / STEP 5. Jen_Moderator |
Follow us on