1/27/2023 5:23 PM | |
Joined: 1/21/2013 Last visit: 9/12/2025 Posts: 4108 Rating:
|
Hello, first we need to know which software controller is installed on your SIMATIC Box PC. On an older PC this would be WinAC RTX, on a newer PC it might be S7-1500S. The best way to monitor the PLC program is to use the original project files. If these are not available, you can try to load the program onto your PC. If your PLC is a WinAC RTX, the uploaded program code will be without text and symbolic names. To upload from a S7-1500S to the TIA Portal, you need the version of the TIA Portal that was used for the download. Further information can be found in the FAQ 'In STEP 7 (TIA Portal), how do you load the "Program Blocks" with the PLC tags and PLC data types from the CPU into the programming device?' and the referenced sources. Kind regards |
1/30/2023 5:48 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
dpends on the installed SW on the PC is there a SW Controller installed? |
Follow us on