7/27/2017 9:54 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003)
|
Hello, how the devices are connected/wired?can you make a schematic Network overview? Regards Christoph |
7/27/2017 10:04 AM | |
Posts: 29 Rating: (0) |
plc and v90 (the servo is connected via ethernet directly to v90.. shouldnt be a problem) are connected via profinet. I can ping both devices from pc. |
7/27/2017 10:09 AM | |
Posts: 29 Rating: (0) |
Device name is the same, error lights are blinking on plc |
7/27/2017 10:19 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating: (3003)
|
and the other things? |
7/27/2017 10:25 AM | |
Posts: 29 Rating: (0) |
I added an edit. Is there something else i need? |
Follow us on