9/1/2022 12:31 PM | |
Joined: 12/11/2018 Last visit: 11/24/2022 Posts: 2 Rating: (0) |
Hello, I have no experience with S5, but have a converting machine that has a problem with the S5 PLC. This PLC is in Stop, I can toggle switch to put into run but no outputs are coming on., If I cycle power to PLC it will again be in Stop. I have Simatic OP7 connected with PLC and the display reads "Verify Loaded Data". Also the LED for battery off/low is illuminated. I am thinking that this PLC has lost its programme, can somebody confirm if this is likely the case? Thanks in advance AttachmentS5.docx (731 Downloads) |
Last edited by: TobyWBB at: 09/01/2022 12:33:08 |
|
9/1/2022 1:17 PM | |
Joined: 12/18/2014 Last visit: 11/18/2024 Posts: 34239 Rating: (4263) |
I hope with you ... |
Follow us on