11/6/2023 9:46 PM | |
Joined: 9/3/2023 Last visit: 11/6/2023 Posts: 2 Rating:
|
Good afternoon, everyone. I'm developing a program for a machine where I have a conveyor belt that needs to move in 76.2mm steps. I'm following the example from this link with EPOS "https://support.industry.siemens.com/cs/de/en/view/109747750." I searched here in the forum to see if anyone was facing the same issue as me, but I couldn't find any. I'm using TIA V18, and the problem I'm facing is that when I power off the machine, the servo doesn't resume from where it left off; I have to reference it again. Can someone help me with this? Here's the link to the program:https://drive.google.com/file/d/12vGedpa-BGNzsiVeFDhm82w4AM2v5JE0/view?usp=drive_link. Grateful. |
Last edited by: Jen_Moderator at: 11/07/2023 09:08:48Link optimized. |
|
11/6/2023 9:50 PM | |
Joined: 7/7/2010 Last visit: 8/15/2024 Posts: 15090 Rating:
|
What type of encoder is installed? Absolute encoder configured for linear motion?
|
science guy |
|
11/7/2023 12:30 PM | |
Joined: 6/20/2017 Last visit: 8/15/2024 Posts: 396 Rating:
|
You are using SINA_POS in the PLC Program. In this case you must homing the drive at every power on, even with absolute encoder. (I don't found the V-Assistant configuration, even in the Tia UserFiles folder), so I assume you are using ABS encoder, but I don't know.
|
Last edited by: Gustavo Banchetti at: 11/07/2023 14:02:28Gustavo Antonio Banchetti Brucatori. |
|
Follow us on