8/15/2006 8:38 PM | |
Posts: 25 Rating: (0) |
Hi Late, The machine working now (it working here near 10 years) and is a painting machine that uses 2 IP242A cards for reading encoders. In the attachment file you can see one page of CPU945 documentation that refer to IP242B only. Also I have read the 6ES5 998–0KM21 Release 2 (Counter Module IP 242A With FB 178/179/180/ IP 242B With FB 183/184) completely. Also please see the following link and give me your opinion about it. http://www.plctalk.net/qanda/showthread.php?t=24654 Best regards, B.Najafabadipour Attachment945ENIP242B.PDF (677 Downloads) |
8/18/2006 9:59 PM | |
Posts: 25 Rating: (0) |
Hi Late, Best regards, Attachmentclearcoat.zip (624 Downloads) |
Follow us on