Default Header
(header konnte nicht geladen werden)
6/6/2014 6:58 AM | |
Posts: 288 Rating: (4) |
hello dear friends. i am learning winac rtx and i've written a simple program as an exercise in order to connect winac rtx to wincc flexible RT but i can't and output field in wincc flexible runtime is displayed with "####" characters! by the way there is no cp5611 in "set pg/pc interface" which i can select however before installing winac rtx and simatic net and wincc flexible 2008 the cp5611 was in "set pc/pg interface"! what is the problem? the installed softwares are: simatic manager v5.5 winac rtx v4.6 simatic net 2010 and window xp 2002 sp3 please help me. best regards. http://www.uploadmb.com/dw.php?id=1402030023 AttachmentD:\tmp\upload\program_and_p_o.zip (202 Downloads) |
Last edited by: CS Moderator at: 8/30/2014 9:26 AMUpload as attachment |
|
6/6/2014 8:00 AM | |
Posts: 8946 Rating: (999) |
The Station has to be a WinLC RTX and you can only select "Softbus" for connection. |
Follow us on