5/25/2021 2:22 PM | |
Joined: 12/18/2014 Last visit: 9/6/2025 Posts: 35929 Rating:
|
What you mean is the article number. If your case it 6ED-1052-XXX08-0BA0. The marked part "08" indicates that there is a LOGO! 0BA8, called LOGO! 8.2. It's a LOGO! 0BA8, device series LOGO! 8.2. Delivery release LOGO! 8.2 |
5/25/2021 2:53 PM | |
Posts: 4 Rating:
|
Yes 6ED1052-2MD08-0BA0 on the logo!, 6ED1055-4MH08-0BA0 on the TDE and logosoft 8.2. Still, if the answer is that the cursors don't work that way I'll just put some external switches on, have to admit I didn't realise it was an 8.2 version, I just bought the starter kit from RS to play with as work has been slow and I thought a vastly over engineered light switch would pass some time and be a fun project.
|
Follow us on