Default Header
(header konnte nicht geladen werden)
2/23/2011 8:01 AM | |
Posts: 4 Rating:
|
I wanted to know if there is any way to communicate a PLC (for example S7-400) with Teleprem XP and collect all tags and data available on TXP? |
3/27/2015 7:50 AM | |
Posts: 11 Rating:
|
Teleperm XP now called as SPPA T2000. The
TXP using application program APRED for redundant communication between
CPU (AS620B-S5) and external system.communication protocoluse ISO
Transport Protocol with Send/Receive . i did it in my plant already, so
yuoneed as follow 1. Complete S7-400 set included with CP 443-1 (the latest Version is 6GK7443-1EX20-0XE0). 2. Buy application software APRED-S7 for S7-400 (MLFB 2XV9450 1AA06). also available APRED S7 for S7-300 (MLFB 2XV9450 1AA07). 3. Follow the manual of the APRED software irkham irkhaju@yahoo.com |
Follow us on