Default Header
(header konnte nicht geladen werden)
11/12/2007 10:49 PM | |
Joined: 10/17/2007 Last visit: 9/12/2025 Posts: 4449 Rating:
|
COMMUNICATION WITH OPM2 for MM3xx Can someone give me some help, I make the wires followed the diagram from Siemens OPM2 manual(see attach.). I am trying to use SIMOVIS in PC to communicte with MM3xx via OPM2 which has the fuction of RS232-->RS485. But I failed. I connected the extenal DC 6V PS by the way. thanks in advance. AttachmentOPM2_Manual_326_B_76.pdf (415 Downloads) |
If you like my comments please |
|
Follow us on