1/2/2017 4:41 PM | |
Posts: 6 Rating:
|
Dear Sir We have Rockwell automation with 1756 L63 PLC connected through Backplane with 1756 CNBT Control Net Card and 1756 ENBT Ethernet Card. All RIO stations and 1395 DC drive controllers are connected via Control Net. Now we got one Siemens 6RA80 Dc Drive Controller of Profibus support which need to be connected with the other drives in the control Network. So how to connect the profibus Drive to the Control Net of Rockwell PLC. And also how to configure the CW, Speed Ref, Current Ref, SW, Speed FB and Current FB of 6RA80 Drive to Rockwell PLC. Pl kindly give me some idea. Waiting for your replay With Regards Pradeepkumar ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/3/2017 9:56:10 AMNew subject after splitting |
|
1/3/2025 6:40 AM | |
Joined: 10/7/2024 Last visit: 9/9/2025 Posts: 2 Rating:
|
Hi any update on the above query? Is the communication done between Rockwell PLC and 6RA80 Drives on Profibus. |
Follow us on