3/6/2023 4:53 PM | |
Joined: 3/27/2008 Last visit: 9/11/2025 Posts: 1216 Rating:
|
When the first Micromaster MM440 was designed there was a plan to make the DC Link able to have a DC Link choke fitted, the attached drawing shows a link where this could be fitted in seriese with the DC line. this option was dropped for later versions. A DC link choke is able to reduce the harmonic effect of the input rectifier on the supply, more effective for larger devices than this 250Watt unit. Loads which posess high referred inertia, a flywheel for example, are difficult to manage when reducing the speed; as the frequency reduces below the speed of the flywheel the motor becomes a generator increasing the Voltage of the DC link beyond acceptable level, causing the inverter drive to trip with Over Voltage, with F0002 displayed. This effect can also be seen when mechanisms are required to ramp down very quickly. A braking resistor if fitted, enables the inverterdrive to dissipate this surplus energy. If your application is able to ramp down without tripping with F0002 (OverVoltage) then a resistor is not required. Tractor AttachmentOld MM4 diag2.docx (707 Downloads) |
Last edited by: Tractor at: 03/06/2023 16:56:54Tractor |
|
This contribution was helpful to
1 thankful Users |
Follow us on