Default Header
(header konnte nicht geladen werden)
5/14/2012 3:22 PM | |
Posts: 3 Rating:
|
Hello! I'm trying to enable and control drive positioning by using Drive Control Charts (DCC) in Starter v4.2. The drive is Sinamics S120 CU310DP , the motor is standard 1LA7 induction motor (1.1kW). The idea is to disable PI controller that is allready in use in Starter -> Position Controller (please see figure 2. in PDF in attachment ) and to use PI controller from the DCC (please see figure 6. in PDF in attachment). The questions are: 1) How to disable PI controller in Starter -> Position Controller? 2) Do you have any examples of position controling from DCC? 3) Is there any possibilities for continuous reading and writing drive parameters in DCC (blocks RDP and WRP do their job but only when "RD" or "WR" are set to 1)? 4) Any other suggestions for this project? Tnx :)
AttachmentPosition controller using DCC.pdf (301 Downloads) |
Follow us on