Default Header
(header konnte nicht geladen werden)
5/20/2016 8:40 AM | |
Posts: 1 Rating:
|
Hello. I use Step 7 V5.5 SP4. There is a problem , the project has FV458-1DP module, but when you open the Hardware says that an earlier version of the database and there is no such unit , and removes them from the hardware configuration . Completed Update HardWare, but says the same thing when UPDATED not find this equipment . What to do? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/20/2016 1:02:24 PMNew subject after splitting |
|
5/20/2016 12:19 PM | |
Joined: 8/25/2006 Last visit: 9/15/2025 Posts: 2218 Rating:
|
Hello. Do you have D7-SYS software installed? |
Follow us on