5/18/2025 1:52 AM | |
Joined: 3/30/2014 Last visit: 5/21/2025 Posts: 102 Rating:
|
For example, this curve is composed of 5 points, which are X1=0, Y1=Var, X2=50, Y2=0, X3=240, Y3=0, X4=303, Y4=Var, X5=360, Y5=Var, and OffsetX=117,Var =100.0. When LAPosition=420, the value obtained by _getCamLeadingValue is 117. if LAPoistion≥50 and ≤ 212, the value obtained by _getCamLeadingValue is always 167. if LAPoistion>212 and ≤ 357, the value obtained by _getCamLeadingValue is always 357. When I modified value of Var to 90.0, the value obtained through _getCamLeadingValue became correct again. This is why I think the _getCamLeadingValue command might have entered some kind of bug state. Software is Scout TIA 5.6 This Cam created by LCamHdl. |
Last edited by: o0yuming0o at: 05/18/2025 01:54:03Last edited by: o0yuming0o at: 05/18/2025 01:56:26Last edited by: o0yuming0o at: 05/18/2025 02:06:00Last edited by: o0yuming0o at: 05/18/2025 02:12:40Last edited by: o0yuming0o at: 05/18/2025 02:18:35Last edited by: Moderator_Lan at: 05/19/2025 06:32:52link optimized |
|
Follow us on