7/8/2025 1:00 PM | |
Joined: 2/1/2010 Last visit: 9/12/2025 Posts: 212 Rating:
|
Since we can't see your screenshot, I'm going to assume you are trying to install just the update first, so: You must purchase IL 9.1 using one of the part numbers listed here: You can't install the SP or any updates from the updates page without the base product installation first. So after doing above, then you can apply the appropriate updates. SIMATIC PCS 7 Libraries Updates Other possibility, if made wrong assumption about missing screenshot: |
If my post helped you, please rate. Thanks. |
|
7/9/2025 8:37 AM | |
Joined: 12/15/2024 Last visit: 7/16/2025 Posts: 8 Rating:
|
THANKS DEAR HOW CAN I SEND YOU SCREENSHOT OF MY ERROR HERE??? WHY I CAN'T ATTACH PHOTO HERE!!!!!!!!! |
7/9/2025 9:08 AM | |
Joined: 7/30/2024 Last visit: 9/15/2025 Posts: 947 Rating:
|
Hello AutoGen_8690, I'm sorry for your inconvenience. It is currently not possible to attach images to posts in the new forum environment. To send attachements, you have to navigate to the classic forum using the button in the green banner on the top of the page. Alternatively, you can open this link and navigate to your topic: https://support.industry.siemens.com/forum/ Kind regards, Moderator_Lan |
This contribution was helpful to
1 thankful Users |
7/9/2025 1:20 PM | |
Joined: 2/1/2010 Last visit: 9/12/2025 Posts: 212 Rating:
|
See my previous post. That is the message you get if you are trying to install IL 9.1 SP1 or the UC media before you installed the base IL 9.1. It must be installed incrementally. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
7/9/2025 8:44 PM | |
Joined: 2/1/2010 Last visit: 9/12/2025 Posts: 212 Rating:
|
You can confirm all the features provided by the library under the manuals. SIMATIC Process Control System PCS 7 PCS 7 Industry Library for PCS 7 (V9.1 SP1) |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to
1 thankful Users |
Follow us on