3/31/2014 8:32 AM | |
Joined: 2/15/2012 Last visit: 5/27/2025 Posts: 57 Rating:
|
Hi, I have several IPC427B and C models running. For the new winccflexible SP3, it is required to install SP3 on windows XPembedded. Where can I find this software? Does Siemens provide a download or do I need to take it from microsoft? Like: http://www.microsoft.com/en-us/download/details.aspx?id=3740 Is this the good version for the microbox series? Thanks in advance, Coldrestart. |
3/31/2014 1:20 PM | |
Posts: 1299 Rating:
|
Hello, see http://www.siemens.com/kompatool WinCC flexible 2008 SP3 is supported for Windows XP embedded SP2. As far as I know there is no SP3 for Windows XP embedded K!ke |
Last edited by: K!ke at: 3/31/2014 1:21 PM |
|
4/1/2014 8:25 AM | |
Joined: 2/15/2012 Last visit: 5/27/2025 Posts: 57 Rating:
|
Hello, I now did the test, see picture in attachment. Installation setup for wincc flexible 2008 SP3 (engineeringsoftware + runtime, but i only need the runtime) I have a brand new windows XP embedded SP3 system, and it doesn't work. When i go manually to the setup for the runtime, i can install the software. But when i open the runtime loader, i get also an error that the installation failed. See attachment 2. AttachmenterrorsWinCC.zip (344 Downloads) |
Last edited by: coldrestart at: 4/1/2014 8:39 AMOK, now i understand it, there is a separate installation DVD/CD for the runtime and the engineeringsoftware.... In the days of protool you can just choose what you needed at the setup, nothing special.... http://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=57267466&nodeid0=16502367&switchLang |
|
4/2/2014 11:16 AM | |
Posts: 1299 Rating:
|
Hello, I think this FAQ helps you: http://support.automation.siemens.com/WW/view/en/40237764 K!ke |
Follow us on