Default Header
(header konnte nicht geladen werden)
5/19/2006 3:37 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hi, The following link is a manual of the MM420 http://support.automation.siemens.com/WW/view/en/19280476 Parameter 1001, 1002 etc are fixed frequencies. Selectable with a digital input. Also look at par. 1070 (main setpoint) When you select 23 at par. 1000, your main setpoint is the fixed frequencie and the analog signal is the additional setpoint. Best regards, Wizard |
Follow us on