Default Header
(header konnte nicht geladen werden)
9/9/2008 10:22 AM | |
Posts: 2930 Rating:
|
Hi, here is a link to the manual of your Air damper actuator: http://www.siemens.fi/cmssbt.nsf/all/AE559AAC6AF7501AC225735F005B8EFF/$file/GSD_GQD.pdf As I understand (I'm not an expert for HVAC market) Connect Red to +24V, Black to Ground and Grey to LOGO! AM2 AQ V1+. Additional connect Ground, Black and LOGO! AM2 AQ M1 together to have the same potentials. Funktion: LOGO! AM2 AQ output value is 0 --> Motor possition closed LOGO! AM2 AQ output is max (10V) --> Motor possition open LOGO! AM2 AQ output is 50% (5V) --> Motor possition is 50% open Here an example created with the older LOGO!Soft Comfort V5. Start the Simulation and play with the inputs. If you want to change the values then change the properties of the analoge multiplexer. I hope this heps AttachmentAir damper actuator.zip (577 Downloads) |
9/9/2008 1:06 PM | |
Posts: 5 Rating:
|
Hi Helmut_13, Thank you for the indications and the example. That will help me. Have a nice day. |
Follow us on