9/8/2015 6:00 AM | |
Posts: 6 Rating:
|
Dear All, Currently I am facing some issue on how to connect the PC to Sinamic DCM. I have found one pdf online that show how to create a RS232 cable to connect both PC and Sinamic DCM. I tried to make the cable and link both the PC and the Sinamic DCM but failed since I have not change the parameter setting. I check my parameter in the BOP, it did not show any parameter code for changing the access level (P0003). Any suggestion for this problem or any method can suggest to me? Thank you so much all for your help. AttachmentSinamic DCM.pdf (1611 Downloads) |
9/8/2015 7:10 AM | |
Joined: 8/25/2006 Last visit: 8/22/2025 Posts: 2218 Rating:
|
Hello. Did you select Drive object 1 (DO1 - CU) using BOP? p0003 exist only in DO1. Look at the manual, chapters 8.2.2, 9.2.2, 8.4.2.4. |
9/9/2015 6:35 AM | |
Posts: 1529 Rating:
|
Also a very common error is the cable. Make sure RX is connected to TX and TX to RX, not TX-TX and RX-RX. |
9/10/2015 4:49 AM | |
Posts: 153 Rating:
|
this seems to be problem with baud rate setting in either laptop or Drive |
Follow us on